Frequently Asked Questions
Please click each question to get the answer.

Order Confirmation Email


1. What is my Download ID and what does it entitle me to download?
Your Download ID is the concatenation of your Rockwell Order Number and Sold To Business Partner ID. This entitles you to download the current version of all software products on your order from the date the order was processed, plus any older versions that are still available for download.
2. How long or how many times can I use the download link in my email?
There is no limit to how long or number of times you can visit the download page with your Download ID. The download page is the one place where you can always go to download the products you purchased, plus any updates, patches, firmware, add-ons, etc. for your product. Note: Product updates may require a support agreement.
3. Can I download software to more than one computer?
Yes, you can download software that you purchased more than one time and to more than one computer. However, you can only install and use the software in accordance with the Rockwell Automation End User License Agreement for the number of activations purchased.
4. Will I continue to receive my software products on disk?
Yes, for now, Rockwell Automation will continue to ship physical media for all software orders, in addition to making products available for download. In the future, physical media may become an option that can be specified on your order.

Download Page


1. Why do I need to agree to the "End User License Agreement"?
The "End User License Agreement" is required to download all Rockwell Automation products. This ensures that you are aware of the rules and regulations required when you download, install, and activate Rockwell Automation products.
2. Are all products available for download?
No, not all software products are available for download. Older products can be removed for the download site. Some products can be removed from the download site on a temporary basis.
3. Can I download an older version of a software product?
Older versions of our software products are available on the download page for as long as they are supported. The number of supported older versions varies from product to product.
4. Is the software I download identical to the software I receive on disk?
For most products, the software on the download page is the same build that ships on disk. Larger products that ship with multiple disks may, in addition to the full product download, offer a smaller "Lite" download option that doesn’t include as many extras.
5. Can I download patches, firmware, product add-ons, etc. from the download page without downloading the product?
Yes, these items can be found under the "Optional Download" section of the download page. To individually download items, click on the item description.
6. Are the optional downloads I select and download with my product installed automatically?
No, optional downloads are provided with their own installation programs and must be installed individually.
7. Can I download multiple products simultaneously?
Yes, use the check boxes on the left to select multiple products. The products download together when you click "download now".
8. Why are some items marked as Not Available?
Items selected from a download page or Product Compatibility and Download Center are almost always be available for download. If you click a link from some other web page, or have stored a download URL and click it later, you may encounter items that are marked as "Not Available". This indicates that the item has been disabled from being downloaded for some reason. You can download only the "Available" items.
9. Can I queue multiple downloads?
Yes, once the Download Manager is running, you can start another download and that download is placed in a queue. After the first download is complete, the next starts.
10. What do I do when I receive "Unable to access your user profile data"?
See Technote 564577 in the Rockwell Automation Knowledgebase for instructions on resolve this error.
11. What do I do when I receive "Unable to Save Basket Info"?
See Technote 638389 in the Rockwell Automation Knowledgebase for instructions on how to resolve this error.
12. Where can I find additional information about download basket?
See Technotes 1027511, 1027513, 1027524, in the Rockwell Automation Knowledgebase for addition information about the download basket.

Software Updates


1. When I enter my serial number and company name, I am told that I do not qualify for an update?
Your serial number is out of support. Please contact technical support to make arrangements for a new support agreement or to extended your support agreement.
2. Why is the "type ahead" performance slow when I search for text or catalog numbers in PCDC?
Your firewall can affect performance. Add "compatibility.rockwellautomation.com" to your firewall's exclusion list.

Download Manager


1. Which web browsers and operating systems are supported by the Download Manager ?
The Download Manager fully supports Internet Explorer version 6.0 to 10. If you have IE11, add 'rockwellautomation.com' to the 'Compatibility View Settings' under Tools menu. If you are using Chrome with Java 7 Update 51 and above, please go to Start > Control Panel > Java > Security, and adjust the Security Level to Medium and add http://download.rockwellautomation.com to Exception Site List. The Download Manager also supports Firefox version 3.0 and higher, and can be installed on Windows XP, Windows Vista, and Windows 7 operating systems. At this time downloads are not supported on mobile devices.
2. What do I do if my web browser or operating system version is not supported?
Media kits are available for all products. Please contact your local distributor or Rockwell Automation sales representative for more information.
3. What languages are supported by the Download Manager?
The Download Manager interface displays in English, unless the Windows operating system is set to one of the following languages: Chinese Traditional, French, German, Italian, Japanese, Korean, Norwegian, Spanish, and Swedish.
4. How do I install the Download Manager?
The download manager can be installed via ActiveX control (Internet Explorer) or XPI (Firefox). In addition, the download manager can be installed via Java or exe. Note: Administrative privileges are needed to install the download manager on your computer. Please contact your system administrator if you are unable to install the download manager with one of these options.
5. What is the default download folder?
The default download folder is the current user’s Downloads folder, which varies by Windows operating system version.
6. Can I change the download folder?
Yes, you can change the download folder, even as files are being downloaded.
7. What is the difference between Managed Download and Direct Download?
Direct Download lets you download one or more files without installing the Rockwell Automation Download Manager. Files download direct to the default Downloads folder. Managed Download is preferred method because it is secure, verifies file integrity, and handles a wide range of communication problems. Managed Download places the files into a predictable folder structure.
8. Are there extra steps with a Direct Download?
Each Direct Download displays instructions for each file. Some files require no action. Typically, larger Direct Downloads come as file sets, where there is a single .exe and one or more .rar files with similar names. Double click the .exe to extract all the files into a folder on your computer. You do not need to double click the .rar files.
9. What do I do if there are multiple files in a Direct Download?
You need to click each file link to download each file separately. Use Managed Downloads, a third party download manager, or see Technote 603590 in the Rockwell Automation Knowledgebase for instructions on how to automate direct downloads.
11. How do I find my files after the download is complete?
When the download is complete, the drop down menu on the "Close" button contains a selection to open the download folder.
12. Why don’t I see files being downloaded to the download folder while the download is in progress?
Files are first downloaded to a temporary location; then they are decompressed and extracted to the specified download folder.
13. How do I know when the download is complete?
When the download is complete, the button in the lower left corner of the Download Manager window changes to "Close".
14. How do I know if there were any errors during the download? What do I do if an error occurs?
The "Status" column in the Download Manager window displays any error messages. If the error can be corrected, you can restart the download by returning to the download page or clicking on the original download link. If you cannot correct the error condition, please contact Rockwell Automation Customer Support for further assistance.
15. My product was downloaded to a folder based on a naming convention. How do I interpret the folder name?
The Download Manager creates a folder for each product, as well as a sub folder for each media image. If you want to keep all of the product images in the same location, you can build a library of Rockwell Automation software products over time if you download to the same location. The media folder naming convention includes the product version, product name, language (other than English), platform (other than protected), special build indicator, and media type.
16. Do I need a third-party program to decompress or extract the files I download?
No, the Download Manager automatically decompresses and extracts the files and places them in a folder structure by product and media image. You can then copy the media image folder to another location, burn it to a disk, or run the installation program.
17. What does "click here if you are using a third party desktop download manager" mean?
If your corporation requires you to use a specific download manager, this link can help. This link is for your convenience only, as no third party download managers are tested or supported by Rockwell Automation. See Technote 603590 in the RA Knowledgebase for instructions on how to use the free WGet utility to automate direct downloads.
18. My download is slow. How do I make it go faster?
Rockwell Automation download images are stored on a global high-speed network of servers. In most cases the files you download come from a server in the same country, or even the same city. Slow downloads can be the result of your Internet connection speed, firewall restrictions, or virus scans. Please contact your system administrator.
19. How do I restart my download after a lost network connection, power failure, or some other problem?
The Download Manager automatically recovers from short or intermittent network connectivity issues. However, if your download is completely interrupted you have to restart the download by returning to the download page or clicking on the original download link. Note: If the Download Manager finds partial files from a previous download, it resumes the download from that point.
20. How do I stop a download already in progress?
You can stop a download in one of three ways: (1) Press Alt-F4, (2) Click the "Close" button in the upper right corner of the Download Manager window, or (3) Click the download icon in the upper left corner of the Download Manager window and select "Close".
21. The computer I want to install my download on does not have an Internet connection. How do I move my download to another computer?
After the download is complete, navigate to the download folder and copy the media image to a remote computer or removable storage device (such as flash drive, memory card, CD, or DVD)

Registration and Activation


1. Does my existing license and activation work with newer versions of software?
Generally speaking yes. Most of older activations work with newer versions of our software products.
2. Do I still have to activate my software after downloading?
Yes, downloaded product media images require activation after they are installed.
3. How do I activate my software?
You register and activate your software by using the FactoryTalk Activation Manager that was installed along with your product or from the activation website at https://activate.rockwellautomation.com/.
4. Do I have to remove my activation first before I update my software?
No, updates can be installed to an already activated product without the need to re-host the activation.
5. Can I activate with a master disk?
No, Rockwell Automation no longer supports master disk based activations.